(0)| 9/26/2022 2:02 PM | |
|
Joined: 8/11/2021 Last visit: 12/18/2025 Posts: 4 Rating:
|
Hi is there any solution to fix this problem? ----------------- SIMATIC IOT2050 SE-Boot Version: V01.02.01-0-g4524e967-0x0000 BuildDate: 20211221 SYSFW ABI: 3.1 [version: 21] [21.5.0--v2021.05 (Terrific Llam] AVS@[1100 1160 1160] ======================= Board: IOT2050-ADVANCED-PG2 Serial: P4CG9116 MLFB: 6ES7647-0BA00-1YA2 UUID: 23504AB0F073439FA91CC98C27521DAF A5E: A5E508877150AB07 MAC[0]: 8c-f3-19 MAC[1]: 8c-f3-19 SKU: SE Loading PK... ok PK count: 00 PK version: 00 SV: 00-00 Security ID 0xc8beb00d-0x7f55c02e Security policy: soft Loading image atf... Loading image tee... Loading image spl... Loading image k3-am65-iot2050-spl.dtb... NOTICE: BL31: v2.5(release): NOTICE: BL31: Built : 14:41:24, May 17 2021 I/TC: I/TC: OP-TEE version: 3.12.0 (gcc version 10.2.1 20210110 (Debian 10.2.1-6)) #1 Wed Jan 20 17:48:48 UTC 2021 aarch64 I/TC: Primary CPU initializing I/TC: Primary CPU switching to normal world boot U-Boot SPL 2021.04-V01.02.01-0-g40d3fc0 (Jan 05 2022 - 14:11:27 +0000) SYSFW ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam') Trying to boot from SPI U-Boot 2021.04-V01.02.01-0-g40d3fc0 (Jan 05 2022 - 14:11:27 +0000) Model: SIMATIC IOT2050 Advanced PG2 DRAM: 2 GiB WDT: Not starting MMC: sdhci@4f80000: 1, sdhci@4fa0000: 0 Loading Environment from SPIFlash... SF: Detected w25q128 with page size 256 Bytes, erase size 64 KiB, total 16 MiB OK In: serial Out: serial Err: serial USER button pressed - booting from external media only Net: No ethernet found. Hit any key to stop autoboot: 0 starting USB... Bus usb@10000: Register 2001040 NbrPorts 2 Starting the controller USB XHCI 1.10 Bus usb@10000: Register 2001040 NbrPorts 2 Starting the controller USB XHCI 1.10 scanning bus usb@10000 for devices... 1 USB Device(s) found scanning bus usb@10000 for devices... Device not responding to set address. USB device not accepting new address (error=80000000) 3 USB Device(s) found scanning usb for storage devices... 0 Storage Device(s) found Device 0: unknown device Device 1: unknown device Device 2: unknown device MMC: no card present IOT2050> Thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: Jojo1000 at: 09/26/2022 14:07:39Last edited by: Jen_Moderator at: 09/27/2022 08:12:03New subject after splitting |
|
| 9/26/2022 2:15 PM | |
|
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi, did you run the IOT2050 out of the box and the STAT LED is red now? The eMMc is still empty, as there is still no IndOS available for the FS:04 devices. So you need to run the Example Image V1.2.2 from SD card or transfer it to the internal eMMc (as described here). For the first tests I would rather run it from SD card, as it is much more easy to reflash the SD card than the eMMc. Best regards! |
|
Not working for IOT2050 support anymore from March 1st, 2024. |
|
| 9/27/2022 8:13 AM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject Boot from USB Stick not possible is published within the conference IOT2050. Jen_Moderator |
Follow us on