8/30/2018 9:54 PM | |
Joined: 8/2/2018 Last visit: 12/16/2023 Posts: 302 Rating:
|
Thank you very much ixo65!! I understand now. ...sent from App |
This contribution was helpful to
1 thankful Users |
10/5/2022 1:47 AM | |
Joined: 12/18/2014 Last visit: 9/17/2025 Posts: 35967 Rating:
|
The resistor parallel to the analog input. The sensor and the LOGO! must have the same power supply. In attachment a picture of example for connecting a two wire sensor to the analog input on connector I7. AttachmentAnschluß Sensor 4 bis 20 mA an LOGO! 0 bis 10 V (I7).pdf (1078 Downloads) |
This contribution was helpful to
4 thankful Users |
Follow us on