10/10/2022 4:55 PM | |
Joined: 1/17/2006 Last visit: 7/14/2025 Posts: 554 Rating:
|
Hello ! I have an application that uses servomotor 1FK7062-3BF71- and a Sinamics S120 drive 6SL3210-1PE16-1AL1 (2.2kW/5.9A) with a Motion-Connect 500 power cable of 85 meters 6FX5002-5CG12-1JF0 4x2.5mm². Now I need the same application but for a distance of 140 meters. My question is if I use a larger drive 6SL3210-1PE22-7AL0 (11.0kW/26.0A) to attend up to a distance of 150 meters (according to D21.4) can I use the same cable 4x2.5mm² with 140.0m ? (6FX5002-5CG12-2EA0) Regards, Berg ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/11/2022 05:21:30New subject after splitting Last edited by: Berg at: 10/11/2022 12:00:26added attachment |
|
Follow us on