11/23/2022 9:46 AM | |
Joined: 10/11/2006 Last visit: 9/5/2025 Posts: 6038 Rating:
|
Hello, with Basic Positioner it is possible to activate position tracking. 8.23 Position tracking Overview Position tracking enables the load position to be reproduced when using gearboxes. It can also be used to extend the position area. https://support.industry.siemens.com/cs/ww/en/view/109781535 With S7-1500 PLC position trackink at the TO (Technologyobject) is possible, too. Choose encoder type "cyclic absolute". |
With best regards, |
|
This contribution was helpful to
1 thankful Users |
Follow us on