(0)| 12/7/2022 4:41 PM | |
|
Posts: 2 Rating:
|
Hi, I have two fairly identical circuit diagrams (CD1 and CD2) for logging data from analogue inputs. When I upload CD1 from my PC to LOGO, the data log module is missing in the program in LOGO itself. The program can be started, but obviously no data can be logged. When I try to download the program from LOGO back to the PC, following message pops up: "Layout restore error. Use the default layout." The data log module is also missing in the downloaded circuit diagram. But using the CD2 everything works as expected: data log is saving data, no error messages etc. Any idea where the problem is? Thanks AttachmentCircuit diagrams.zip (498 Downloads) |
| 12/7/2022 5:02 PM | |
|
Joined: 12/18/2014 Last visit: 12/29/2025 Posts: 36382 Rating:
|
There is something corrupt in the file CD1. The Data Log block is only named "L" from the software, not "L1" as in CD2. Why? Start a Support Request and ask Siemens directly. |
Last edited by: ixo65 at: 12/07/2022 17:13:06 |
|
| 12/7/2022 5:14 PM | |
|
Posts: 2 Rating:
|
No idea. The name of the block is given automatically when I place it into the layout. |
Follow us on