(0)| 5/9/2009 8:59 PM | |
|
Posts: 1742 Rating:
|
Hello, I am not sure that I have undertood you well. Scalance S can be used in two modes (both supporting the setup of VPN) - in routing mode (which is the mode when you run over Internet for instance) - in bridging mode (you have a flat network) I guess that you refer to the second mode, where several systems are in one network but you want to protect the automation cell via Firewall and VPN tunnel. An example of this is available here: http://support.automation.siemens.com/WW/view/en/22056713 But if you run over Internet, the routing mode is mandatory. |
Last edited by: edr at: 5/9/2009 9:30 PM |
|
Follow us on