12/26/2022 2:06 PM | |
Joined: 4/8/2009 Last visit: 9/8/2025 Posts: 35 Rating:
|
Hi all, I wonder if anybody has been able to provide BOOLEAN data with Modbus Server from S7-1500 The manual could not be prepared more confusing Task is simple. There is a Modbus Client which request with Function 01 or 02. S7 ModServer should provide the values for these requests from the DataBlock connected to the Modserver "databuffer" input. Like for the function 03. Why should we required to deal with conversion from bool to int or vice versa. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/27/2022 07:27:44New subject after splitting |
|
Follow us on