1/16/2023 1:45 PM | |
Joined: 9/5/2022 Last visit: 4/16/2025 Posts: 3 Rating:
|
Hello again yes i have five inverters and each inverter have a five MB_CLIENT block for read different registers(4) and write(1). ı can't upload online parameters right now. because i am not in the field right now. I will upload soon. I don't know what is the problem because when I restart the intelligent device blocks are working true and when the problem occurs i can't read data from plc and i can't read data from Modbus Poll. Modbus Poll giving me error(Read error, Write Error) I tried all the solutions i know disconnect and disable each mb client blocks except one and I used this one and test it manualy. I connect two tag for disable and connect test it but it didn't work. Question is what can be the problem? AttachmentTIA SCREENSHOTS.zip (587 Downloads) |
Last edited by: aakinaayhan at: 01/16/2023 13:58:54 |
|
Follow us on