1/26/2023 12:09 PM | |
Joined: 6/25/2018 Last visit: 3/17/2025 Posts: 15 Rating:
|
Hi, I had the same problem and I'm using the solution proposed by this article: https://support.industry.siemens.com/cs/de/en/view/109794243 Screen Number To keep the current screen number permanently available in a tag, link the "Built" event for all screens with the following code: Tags("Screen Number").Write(Screen.ScreenNumber); Subsequently, the "ScreenNumber" tag always contains the screen number of the current screen. Notes Setting the tag value by the PLC alone does not lead to a screen change of the Runtime. When using screen windows, put the code only in screens with content, but not in pure navigation screens. By default, the screen number in WinCC Unified is 0 for all screens.
|
Last edited by: Jen_Moderator at: 01/27/2023 07:23:00Link optimized. |
|
This contribution was helpful to
2 thankful Users |
Follow us on