2/16/2023 5:50 AM | |||
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Hi, On PROFINET the "slave" is called "IO-Device". The cpu has different ressources for that, which can be found in the technical data. Example: 6ES7315-2EH14-0AB0-> PROFINET IO Controller ->
Please note: There are different versions of the CPU 315-2 PN/DP which may have different numbers! Please check which CPU is used exactly! regards sancruz |
||
Feedback appreciated, please rate |
|||
This contribution was helpful to
1 thankful Users |
Follow us on