2/14/2023 2:06 PM | |
Joined: 11/5/2019 Last visit: 5/22/2025 Posts: 19 Rating:
|
Dear all, I'm using the TCON function to make a connection to a Sick Inspector PIM60. I followed the manual thats avaiable on the Sick site. The camera part is setup fine, but I can't get a connection through the TCON block. I tried using a 3rd party software (Hercules utility) for mocking/testing the connection, but it gives the same result. At first the status will always be 7000, but when I try to evaluate the status I get 80A3 ( Attempt being made to re-establish an existing connection). Even if I change the ip adres to something that doesnt exist, I get the same code. The ip adres of the camera is 192.168.1.20 and of the plc is 192.168.1.30 I'm using tia portal 15.1 and a 1500 (6ES7 511-1AK02-0AB0) Do you know what solutions I can try? Kind regards,
Attachmenttcon.zip (531 Downloads) |
2/15/2023 2:10 PM | |
Joined: 1/21/2013 Last visit: 9/19/2025 Posts: 4114 Rating:
|
Hi TToorn, perhaps a look at the connection details might help. It might also help to use the trace function to see if other status values are being displayed. Kind regards |
Follow us on