2/23/2023 8:43 AM | |
Posts: 26 Rating:
|
Hi all, Im working with a S7-1200 (CPU 1215C AC/DC/RLY) and a MTP700 Unified comfort panel. The IP adress of the PLC is: 192.168.0.22 The IP adress of the HMI is 192.168.0.23 The two are connected via profinet. If i connect the PLC straight to my laptop, i have acces to everything (PLC and HMI). Last week i did not have this issue... Any thoughts on this? Attachmentissue.zip (691 Downloads) |
2/23/2023 9:25 AM | |
Posts: 26 Rating:
|
Hi Towome, If i ping, i get "Request timed out" , im sure there's no other device with the same IP. What setting could it possibly be according to you? |
2/23/2023 10:30 AM | |
Joined: 3/30/2020 Last visit: 9/12/2025 Posts: 5446 Rating:
|
Have a look at the PCs network configuration -- dynamic IP or fixed IP, and which IP (+ subnet) is active. Then the security settings of the PLC is of interest -- especially when having S7-1200 firmware V4.5 or V4.6. Consider reporting all of those to the communication experts. But PING not working.... |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
1 thankful Users |
2/23/2023 3:58 PM | |
Posts: 26 Rating:
|
Ahhhhh crap. Won't make this mistake anymore. Big thanks!! |
This contribution was helpful to
2 thankful Users |
Follow us on