(0)| 2/14/2023 7:03 AM | |
|
Joined: 3/30/2020 Last visit: 12/11/2025 Posts: 5656 Rating:
|
Somewhere you have to specify something like S7-1200 firmware between V4.0 and V4.4 (inclusive) designed in Step7 of V13.0.2.0 to V18.0.0.0. Code is programmed in SCL as to make text file export possible to transplant code to any of the beforementioned Step7 versions. Python compatible with V3.8[1] (or V3.10[2]) -- depending on threading / async concurrency used. The 3rd party software which I mentioned earlier is the most robust. Else you can have a look at sample in the following link: [Interface with S7-1200 using Python] Beyond this point I am not able to assist. [1] - Windows versions after Windows XP |
Last edited by: qwazee at: 02/14/2023 07:09:48Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
|
|
Follow us on