(0)| 5/12/2021 8:22 PM | |
|
Posts: 17 Rating:
|
Hello there, I need your fast help. I have 3 separate s71512F PLCs. I configured 1 of them as I Device and exported the GSD file. I want to configure it by importing this GSD file to the remaining 4 plc. I can connect to a device with a single IO Controller. there is no problem. But when I want to connect with the 2nd IO Controller, I get the attached error. I could not install to I Device with 2 IO controllers at the same time. When one of them connects, the other produces the same error. You can see the architecture I need in the attachment.
AttachmentDoc.zip (655 Downloads) |
| 5/13/2021 1:05 PM | |
|
Posts: 17 Rating:
|
Greetings Einstein!! thank you for your answer. Actually, I want basically that; I have one sensor in "I device" and it is doing a very important measurement. I want to read this integer value from 2 plc files for now. However, only one io controller can be connected. The other IO Controller fails. You can also see the error code in the attachment. The configuration I made on I device is attached. my arrow directions are like this. There is no write command from IO Controllers to I device.
Attachmentdoc2.zip (607 Downloads) |
| 5/13/2021 8:07 PM | |
|
Posts: 17 Rating:
|
Hello, i changed subnet id and io controller. result is same :( you can find attach.. Attachmentdoc3.zip (668 Downloads) |
| 2/25/2023 3:25 PM | |
|
Joined: 11/13/2020 Last visit: 4/16/2024 Posts: 1 Rating:
|
Hey. I have a similar project. Did you solve this problem? |
Follow us on