(0)| 2/17/2023 11:56 AM | |
|
Posts: 10 Rating:
|
Hello I have similliar problem with my drive. Machine type Lathe "Trens SBL500" with simoidrive 810D. One of spindle encoder was damaged Heidenhain on the chunk axis we have replaced that by new one but following errors still exist: 25000 Axis C1 hardware fault of active encoder 25001 Axis C1 hardware fault of passive encoder 300504 Axis C1 drive 3 fault of motor transducer 25201 Axis C1 drive fault But encoders now is working showing both values but something still wrong Then I was trying to change Axis MD 30200 to 0 and 30240 both to 0 and still can't run spindle have these errors: 300504 Axis C1 drive 3 fault of motor transducer 25201 Axis C1 drive fault Another strange detail that after reset error if I move spindlle motor by hand same fault apiers. Seems that system still following encoders or something. Maybe someone can help? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Justass at: 02/17/2023 11:57:18Last edited by: Justass at: 02/17/2023 11:58:15Last edited by: Jen_Moderator at: 02/17/2023 13:21:51New subject after splitting |
|
Follow us on