(0)| 3/2/2023 2:05 PM | |
|
Joined: 10/11/2006 Last visit: 1/16/2026 Posts: 6068 Rating:
|
Hello, maybe you use the false value (sdValue/srValue). 5.2.8.7 Data structure of the "sxParameter" area Note TIA Portal/Startdrive V14 As of TIA Portal/Startdrive V14, the instance data block of the SINA_PARA in the "sxParameter" data structure contains two different input or output fields in the formats REAL and DINT (new!). All of the parameters of the type DWORD or DINT must be written in the sxParameter[x].sdValue field as of this version. The block logic has been modified to the extent that the job field sxParameter[x].sdValue is used for reading and writing for the automatic detection of the DWORD or DINT format. For all of the other parameters, the already existing sxParameter[x].srValue field is used as usual. If this is not the reason, please check the error and status messages. 5.2.8.10 Error handling of the FB286 function block Troubleshooting function block SINA_PARA https://support.industry.siemens.com/cs/ww/en/view/109475044 |
|
With best regards, |
|
Follow us on