11/14/2021 6:31 PM | |
Joined: 2/13/2020 Last visit: 1/28/2023 Posts: 54 Rating:
|
I´m not sure how you have numpad in unified but here is how you can do it from a IO field if that is what you use. |
2/9/2023 9:38 AM | |
Joined: 1/21/2013 Last visit: 9/19/2025 Posts: 4114 Rating:
|
Hi Pratts23,
that is because "Press key" and "Release key" events are not supported on a Unified Comfort Panel. See Notes on the operation of Unified Comfort Panel. Kind regards |
2/9/2023 10:10 AM | |
Joined: 9/22/2014 Last visit: 3/2/2025 Posts: 89 Rating:
|
Hello Mate, I understand the reason why its not working on device , but what is the solution to this ? How can we know enter key is pressed ? How easily it is given in comfort panels with the event "Input finish" where as in Unified i dont get any option. Experts please share any solution. Thanks for the help.
|
3/16/2023 8:05 AM | |
Joined: 1/21/2013 Last visit: 9/19/2025 Posts: 4114 Rating:
|
Hello everyone, The "Input finished" event is now available in WinCC Unified V18, Update 1. To use it, you need to configure the device as V18.0.0.1. Update 1 is also required for the SIMATIC WinCC Unified PC Runtime. If you are using a WinCC Unified Comfort Panel, the update should be available from mid-April. I have already verified the functionality and posted a small example at 'Input finished IO field doesn't work'. Please do not be confused by the title, it works! Kind regards |
This contribution was helpful to
1 thankful Users |
Follow us on