4/5/2023 2:59 PM | |
Joined: 8/12/2021 Last visit: 7/26/2024 Posts: 322 Rating:
|
Hi Kaleelmohamed! I suggest you to check the parameters of the connection setup according to the manual. It is possible that the version of the instruction is not correct. On the other hand the error code may be being overwritten. I advise you to use an error logic (save status in an auxiliary variable when the error is triggered) to see if another code appears.
|
If this Information really helps, you could use the Rate function |
|
Follow us on