(0)| 4/14/2023 2:18 PM | |
|
Joined: 6/29/2022 Last visit: 12/5/2025 Posts: 1 Rating:
|
We have installed the Telecontrol and configure the same based on the project "CP1242-7_SMS_COMPACT_PROJ_V17.zap17". But only one number which is first in the array get the SMS rest no do not get the SMS. Kindly help. Project Attached. AttachmentCP1242-7_SMS_COMPACT_PROJ_V17.zip (554 Downloads) |
| 4/19/2023 11:12 AM | |
|
Joined: 8/3/2009 Last visit: 1/16/2026 Posts: 16644 Rating:
|
Hello Ashish_Rehaan Do you mean this example? https://support.industry.siemens.com/cs/de/en/view/58638283 Or another one, do you have a link or a source? do you get any errors? Used Versions? Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on