(1)| 5/10/2023 7:02 PM | |
|
Joined: 3/13/2012 Last visit: 12/30/2025 Posts: 7 Rating:
|
Same here. How do I add PROFIsafe to the PNPN 6es7158-3ad10-0xa0 coupler in TIAP V15.1? There is no ProfiSafe Type in "transfer mapping" ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/11/2023 09:50:50New subject after splitting |
|
| 5/11/2023 4:54 AM | |
|
Joined: 3/11/2019 Last visit: 12/9/2025 Posts: 1653 Rating:
|
Hi, again, in TIA V15.1 the specific PROFISafe I/O not available when the coupler is configured via integrated hw-catalog (depends on the version of TIA). Or try to configure via GSDML, after installation the coupler is also available in folder "other field devices", but as mentioned above, it is not necessary. PROFINET GSD files : Gatewayregards sancruz
|
Last edited by: sancruz at: 05/11/2023 04:57:32Feedback appreciated, please rate |
|
Follow us on