(0)| 5/11/2023 9:53 AM | |
|
Joined: 3/11/2019 Last visit: 12/9/2025 Posts: 1653 Rating:
|
Hi, there is an application example based on the instructions WRREC/RDREC for i-device communication with data records. Configuration and Application of the PROFINET I-Device Function
Additional note: The formal parameter "ID" of these instructions are used on S7-1x00 and S7-300 differently, please have this in mind. Use the program example of the control data record with WRREC & RDRECWhat restrictions are there for active jobs when communicating with "WR_REC/"RD_REC" and "RDREC"/"WRREC" via PROFIBUS DP and PROFINET IO?
regards sancruz |
|
Feedback appreciated, please rate |
|
This contribution was helpful to
|
|
Follow us on