(1)| 5/10/2023 8:39 PM | |
|
Joined: 3/13/2012 Last visit: 12/30/2025 Posts: 7 Rating:
|
Same here. How do I add PROFIsafe to the 6es7158-3ad10-0xa0 PNPN coupler in TIAP V15.1? There is no ProfiSafe Type in "transfer mapping" ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/11/2023 09:53:04New subject after splitting |
|
| 5/11/2023 4:51 AM | |
|
Joined: 3/11/2019 Last visit: 1/7/2026 Posts: 1653 Rating:
|
Hi, as far as I know, in TIA V15.1 the specific PROFISafe I/O not available when the coupler is configured via integrated hw-catalog (depends on the version of TIA). Or try to configure via GSDML, after installation the coupler is also available in folder "other field devices", but as mentioned above, it is not necessary. PROFINET GSD files : Gatewayregards sancruz |
Last edited by: sancruz at: 05/11/2023 04:56:40Feedback appreciated, please rate |
|
This contribution was helpful to
|
|
| 5/11/2023 9:53 AM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject Add PROFIsafe to the PNPN 6es7158-3ad10-0xa0 coupler in TIA V15.1 is published within the conference Communication / Networks. Jen_Moderator |
Follow us on