(0)| 5/10/2023 12:14 AM | |
|
Posts: 3 Rating:
|
Hello everyone. I would like to ask for advice on my project, namely: To develop an interface in LabVIEW for controlling an electric drive via NI OPC server. The problem is the following:
(look at the picture) Maybe I'm translating addresses wrong somewhere? AttachmentScreenshots.zip (528 Downloads) |
Last edited by: Jen_Moderator at: 05/10/2023 10:32:59All files added as .zip file. |
|
| 5/10/2023 5:35 PM | |
|
Posts: 3 Rating:
|
If I am not mistaken, then according to the nameplate on the engine at a maximum of 1350 rpm, the rated current is 0.42 Arms. But on the graph in LabVIEW, at any given speeds, it jumps 9990,00-9998,00. The S7 PLC acts as an OPC UA client, yes Maybe the types don't match, what I get from the PLC should match the LabVIEW type. AttachmentZIP - WinRAR.zip (530 Downloads) |
Follow us on