(0)| 5/22/2023 6:26 AM | |
|
Posts: 1 Rating:
|
hello Everyone, I need urgent support regarding Diagnostic's alarm generated by asset management system in servers. My client doesn't want to see the alarm in the server and client side. I gave him a option to remove the diagnostics hierarchy so that it will be deleted from the system but he is not accepting this option. Now I need a solution that i will remove the diagnostics alarm from server without doing anything in the AMS or in the main PCS7 Project. PFA Appreciate if anyone can help. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/22/2023 06:41:26New subject after splitting |
|
Follow us on