(0)| 6/7/2023 1:15 PM | |
|
Joined: 3/30/2020 Last visit: 12/11/2025 Posts: 5656 Rating:
|
Andrey, When you make it easy for our volunteers to follow your thoughts then chances increase that field experts will come to discuss this case with you. Not providing linked information reduces your chances for constructive conversation. The original topic you abandoned is published here:S7-1200 PLC collecting data from 4 LOGO’s. Therein the application example (LOGO! - S7 Connection with LOGO! Client and S7-1200/1500 Server) was given to you for study. The application example uses "S7 communication" and direct/absolute addressing. The configuration on the S7-1200 side is made only in hardware configuration. A resource identity is created and the device responsible for making the connection is selected. The LOGO! side the configuration is done via configuration and an assignment table. In the assignment table the absolute addressing is listed for LOGO! against the S7-1200. This reminds of an i-device configuration. The PUT and GET functionality is within the LOGO! and timing regulated by the LOGO! The S7-1200 reacts by background processes to the requests as poled by the assigned resource. Each resource is poled (time slicing) as the CPU chooses. Note that the CPU has a limit to the count of communication resources that it will handle. This limitation ensures that each device can be serviced in a timely manner. One important point: The S7-1200 DBs linked to the LOGO! must not be of an optimized structure. You are welcome to use the "Support Request" link to speak to Siemens directly if this topic does not meet your requirements. Best health. |
Last edited by: qwazee at: 06/07/2023 13:19:20Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on