(0)| 6/9/2023 9:26 AM | |
|
Joined: 1/12/2023 Last visit: 3/13/2025 Posts: 2 Rating:
|
Hello, In our project, we want to have V90 position control with Sinumerik One controller. But we cannot run it. We also have connection problems. Is there a problem of using technology objects in Sinumerik One? Can it be used? We see 2200066 error code on One Operate Screen NOTE: During the studies, both the motor can be moved in simulation mode in Tia V17 and the motor can be moved via V-Asistant, but the movement cannot be provided with blocks. How can we have V90 position control with Sinumerik One Controller ? I kindly ask for your help. Thank you. Best regads, ------------------------------------------------------------------------------------------ |
Last edited by: dmert at: 06/09/2023 09:29:38Last edited by: Jen_Moderator at: 06/09/2023 10:40:32New subject after splitting |
|
| 6/9/2023 10:43 AM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject V90 position control with Sinumerik One controller is published within the conference SINUMERIK CNC automation systems. Jen_Moderator |
Follow us on