(0)| 6/15/2023 12:13 PM | |
|
Posts: 1 Rating:
|
Hello, do you already get a solution for this problem? I've the same problem. I'm working with TIA V.16, IPC627E and S7-1507S Soft-PLC. The UaCPP Server is running on the IPC and the Soft-PLC and the IPC are connected via PROFINET. I've done all steps of the documentation to install an OPC UA client on the PLC. I don't get a connection between the OPC UA client on the PLC and the UaCPP OPC UA Server on Windows. What did you done in the server to establish a connection? I'm getting the error code in diagnostics--> subfunctionStatus: 16#800A_0000. Do anyone know what does this mean? Thanks for your help. Lots of regards Franziska ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_4413456 at: 06/15/2023 12:39:43Last edited by: Jen_Moderator at: 06/28/2023 09:39:05New subject after splitting |
|
Follow us on