(0)| 7/20/2023 1:34 PM | |
|
Joined: 9/27/2006 Last visit: 1/21/2026 Posts: 12481 Rating:
|
Hello; Allthe Profibus and MPI addresses are the same on the CPUs linked in your application. Access to the CPUs is dependant on the MPI addtess. If a single MPI address is attributed to the CPUs, connexions will all try to connect to the closest CPU with that address. See this extract from the Programming with Step 7 system manual: https://support.industry.siemens.com/cs/ca/en/view/45531107 Solution: go back to your HWConfig editor, change the MPI and Profibus addresses in your project si they are unique to each CPU. Save, compile and download the modified hardware configration for each CPU. Then you should have access to each CPU individually. Hope this helps, Daniel Chartier |
Follow us on