(1)| 7/6/2023 8:42 AM | |
|
Joined: 3/14/2008 Last visit: 12/28/2025 Posts: 2233 Rating:
|
Hi, PCS7 V9.0 SP1 has been released for Windows 7 Ultimate x64 SP1. I suggest you start with a fresh copy of Windows 7 and upgrade to SP1 before installing PCS7. |
|
If I could help you, you can use the RATE button. Thank you. |
|
| 7/25/2023 4:52 PM | |
|
Joined: 1/11/2019 Last visit: 11/24/2025 Posts: 899 Rating:
|
Hello Muntadher, Eb=ven I had faced this error in my projects. I installed the TH update (PCS7 TH V9.0 SP1 Upd1 and actually all updates) from the 9.0 SP1 product page and my problems were resolved. Link to download TH V9.0 SP1 Upd1 SIMATIC PCS 7 V9.0 SP1 Software Updates --- What's new in the plant hierarchy (PH)? V9.0 SP1 Compared with the previous version V9.0, version V9.0 SP1 includes the following enhancements or changes: ● The "Repair" button in the "Plant Hierarchy - Settings" dialog can be used to repair the
diagnostics settings and to eliminate the cause for an inconsistency message of the basic
settings of the PCS 7 maintenance station. ---- I hope it works for you! |
Follow us on