(0)| 7/31/2023 5:00 PM | |
|
Posts: 1 Rating:
|
I have the same issue. We are using 7 drive on communication. 6 is working without any issue. Only one drive is not working. At FbDrive Bad parameter value is 1 and ModErr parameter value is 1. This VFD was also working 5 days ago. Suddenly after one power cycle it had stopped working from DCS. Rightnow this is being operated from CDP of VFD. Values at PZDIn1 & PZDIn2 are updating with various values when started or stopped the VFD from CDP. On faceplate it shows "Motor Protection" status, and I am unable to reset it from faceplate. Please advise what should I check. Regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/01/2023 09:06:51New subject after splitting |
|
Follow us on