(2)| 4/18/2023 3:08 PM | |
|
Posts: 2 Rating:
|
Hello i am using s7-1200 plc and siemens v20 drive and i am controlling the drive over RS485 Through uss communication. So i need a feedback a digital output from drive what exact parameters should i put to get Error fault from drive's digital output.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/19/2023 09:04:47New subject after splitting |
|
| 8/1/2023 9:16 AM | |
|
Joined: 10/11/2006 Last visit: 1/19/2026 Posts: 6069 Rating:
|
Hello Thiago Omena, terminals 15&16 are transistor outputs. Those can only handle a certain amount of current, see V20 operating instruction manual chapter 4.2. https://support.industry.siemens.com/cs/ww/en/view/109811111 Also make sure that the digital input of the PLC is using the same reference voltage as the supply you are using for the digital output. |
|
With best regards, |
|
Follow us on