(0)| 8/3/2023 9:57 AM | |
|
Joined: 3/30/2014 Last visit: 10/14/2025 Posts: 88 Rating:
|
Power meter: is the first best that came to my mind. The schedule is a simplified representation. To not make it too difficult. Fixed fact: the energy meter is set with 18000 pulses per 1000 Wh. Pulses come in through I3 in B001. Followed by 2 more Up/Down counters. All do their job nicely. On the other hand, the Threshold trigger B002 also receives this signal. And as of now, I'm probably thinking wrong. I feel there are mistakes. What are the correct values that I should put in B003 (Mathematic Instruction)? Please read to 3 digits after the comma. The why? The software controls other devices at a set power. AttachmentPower meter.zip (600 Downloads) |
Last edited by: Jen_Moderator at: 08/04/2023 06:53:55Text formatting optimized. |
|
| 7/14/2025 4:57 PM | |
|
Joined: 3/30/2014 Last visit: 10/14/2025 Posts: 88 Rating:
|
My solar inverter is a 3-phase 5 kVA inverter. It starts with a TIP Sinus 85 S0 meter (3-phase 230/400 V). The output is 18,000 pulses per kWh. These pulses arrive at I3. The attached diagram is only part of it. I can live with the fact that I only see even numbers. And now I have doubts about the accuracy of the Logo. The solar panel's dashboard shows other, varying values. My question is: Am I doing something wrong in the programming or settings?
Attachmenttest1.zip (138 Downloads) |
| 7/16/2025 10:34 AM | |
|
Joined: 12/18/2014 Last visit: 1/18/2026 Posts: 36470 Rating:
|
Which LOGO! have you exactly? Please write the complete order number? |
Follow us on