(1)| 8/16/2023 6:35 AM | |
|
Joined: 3/21/2019 Last visit: 8/19/2025 Posts: 6 Rating:
|
Welcome everyone! I have created a modbus tcp/ip connection with an electric column. The column is the server, plc is the client. I need to read several registers and write several registers. Communication between plc and column works, I can read and write data. However, I have a problem because I get ERROR and status 80A3 regularly. I've tried to solve it in several ways, but none works. Please support what changes to make in the program so that ERROR 80A3 does not occur. I am sending screenshots and program archive in the attachment. Regards,
Attachmentattachments.zip (530 Downloads) |
Follow us on