(0)| 8/9/2023 8:54 AM | |
|
Joined: 8/25/2014 Last visit: 11/28/2025 Posts: 138 Rating:
|
Hello. Chitokota and others. The comunication principle is the same from what I saw from both manuals. I can't seem to get my head around the message frame that needs to be sent to the energy meter to get the result of the used power. The manual states that the messaga frame should be like this: Physical address: 1 byte - 1 to F7h (1 to 247) So I made a DB with an array of 8 bytes. So if I would want to read the used power from the energy meter I guess I need to send this: Physical address -- Funcion code -- Starting address -- Quantity of registers -- CRC 1 -- 03H -- 0034h -- 2 -- ? The link to the Modbus manual, too see what I mean: https://gavazzi.se/app/uploads/2020/11/em330_em340_et330_et340_cp.pdf Any info on this topic would be great. Thank you. Cheers Aleix ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/09/2023 10:39:55New subject after splitting |
|
Follow us on