(0)| 8/16/2023 10:53 PM | |
|
Joined: 5/26/2022 Last visit: 1/15/2025 Posts: 3 Rating:
|
Hello all, I have a problem with project. The project consists of PLC (S7-1500/1513-1 PN), HMI (TP700 Comfort) and two Sinamics V90 drives for controlling servo motors (X and Y axis). "PROFINET interface_1,For multiple use IO systems or standard machine projects, all specified partner ports are limited to partner ports of their own IO system" I also tried to enable "Multiple use IO system" but error is the same. When I worked on TIA Portal V15.1 I did not have any problems with that, but when I changed to TIA Portal V17 and try to made new project I get described error. Does anyone know how to fix this problem? Thank you in advance! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/17/2023 10:10:07New subject after splitting |
|
| 8/17/2023 10:11 AM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject Multiple Use IO System with Configuration Control is published within the conference Communication / Networks. Jen_Moderator |
Follow us on