(0)| 8/17/2023 5:09 PM | |
|
Joined: 11/21/2017 Last visit: 4/30/2025 Posts: 1 Rating:
|
I am using CPU 1511 and CU320-2 PN (5.2). I have configured telegram, but in the PLC I can only see data from the drive control (IW100...) and infeed (IW370...), but all data is from axis = 0. When I look online, the value in axis telegram value = 0 (in the parameter it has a value =20, for example, temperature). I add the axis parameter to the drive control telegram – it does not work. Physically, everything is fine: when I use acyclic communication , I can see all the parameters.
AttachmentScreenshots.zip (373 Downloads) |
Last edited by: Jen_Moderator at: 08/18/2023 08:42:34All files added as .zip file. |
|
Follow us on