9/4/2023 8:31 AM | |
Joined: 5/6/2022 Last visit: 8/13/2024 Posts: 439 Rating: (86) |
Hi BranoD, I'm afraid this is not possible. An HMI program does not have the possibility of making a comparison with an offline project as can be done with a controller (PLC). The only way or alternative would be to open the program on two different computers and compare object by object. I hope I have been able to clarify your doubt. Best regards! |
If this Information really helps, you could use the Rate function |
|
Follow us on