(0)| 9/14/2023 5:01 PM | |
|
Joined: 3/3/2010 Last visit: 12/17/2025 Posts: 10 Rating:
|
Hi to all, I am writing to seek assistance in establishing communication between a PLC S7-1200 and a soft starter 3RW5224-1AC14 through Profinet. We have the card 3RW5980-0CS00 inserted in the slot of the soft starter. We have created the project in TIA V17, which I have attached. The communication is successfully established, and we are able to go online with both devices. The assigned input and output addresses are: I address: 2...17 Q address: 2...5 However, we are uncertain about what these addresses correspond to. The information provided in the soft starter and Profinet card manuals is not clear on this matter. We are unsure if there is a control and status word. We kindly request your assistance in understanding how to start the soft starter from the PLC and how to assign variables to these addresses. If you have a sample program available, we would greatly appreciate it, as the information provided is quite limited. Thank you in advance for your help. Attachment3RW52_Profinet.zip (490 Downloads) |
Follow us on