(0)| 9/20/2023 10:59 PM | |
|
Joined: 7/11/2023 Last visit: 2/3/2025 Posts: 4 Rating:
|
Any updates on this? I am experiencing a very similar issue with a CP340 dropping communication at unpredictable times. I need a way to either prevent this or recover from this without restarting the PLC. I'm also pretty new to Siemens controllers but I've been able to find the the diagnostics buffer for the CP340 in the hardware config of Simatic Manager but it doesn't seem to give me any information about its serial communication, just that the module is OK and that the PLC is in RUN. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/21/2023 09:30:58New subject after splitting |
|
Follow us on