(0)| 9/20/2023 4:43 AM | |
|
Joined: 4/28/2015 Last visit: 11/27/2025 Posts: 10970 Rating:
|
Hello, I recommend maybe check again initialisation procedure of that scanner, maybe preconfigurate it as is expected with some Sick SW. With upload via different TIA versions I can recommend typical Topic inside Industrail Software Conference: Upload PLC prg - different TIA version reader has a same IP address and copy-paste settings from an old one. We see the device in network, but PLC do not see it. This is what is not clear to me, you've preconfigured this device prior use or you simply describe cfg from PLC cfg options? You see IP of it via what diag option or SW? Can you show us finally some screenshots that shows your device available on 'network' because I don't understand where you have test this? |
Last edited by: Duris_I at: 09/20/2023 04:49:23With best regards... |
|
| 9/20/2023 9:37 PM | |
|
Joined: 8/15/2023 Last visit: 2/11/2025 Posts: 6 Rating:
|
Hi, First of all I preconfigure reader in Sopas: assign correct name, IP address and dozens other settings - so yes, new reader is physically configured the same way as the old one. How can I see it is in network - I configure it through the network hub - if it is not online - how could I do it? I get positive ping reply from the IP I have assigned, so I am 100% sure it is online and IP address assigned correctly. But when in TIA accessible device list I can see PLC, SMC mainfolds, Beijer control panel, Crevis terminals - but not SICK reader... Screenshots - I will make some in couple days. |
Follow us on