(0)| 9/25/2023 1:50 PM | |
|
Joined: 5/16/2018 Last visit: 9/26/2025 Posts: 5 Rating:
|
I'm from Brazil and I'm looking for support from Siemens too. I have an application with 10 thousand tags and 4 connected clients, 2 on each computer (2 windows). WinCC Unified V18 Update 2. Basic supervision, without routines, seeking to use good library practices, light figures and the like. Each tab opened in Chrome consumes 32% of an I7-12700, reaching 48%. The server to which WinCC is allocated has an Intel Xeon 8C/16T, 128gb of ram, top server, Dell. The server is experiencing spikes of 80% CPU usage. Is very. I would like to know how WinCC Unified should behave in an application with 50 thousand tags. Previously used the Elipse E3, infinitely better. I'm talking about a supervisory that contains 200mb versus WinCC that weighs more than 10 gigs. What to do? ------------------------------------------------------------------------------------------ |
Last edited by: agnaldo.junior.br at: 09/25/2023 14:30:14Last edited by: Jen_Moderator at: 09/26/2023 07:53:43New subject after splitting Agnaldo Junior - Computer engineer |
|
Follow us on