(0)| 9/25/2023 2:16 PM | |
|
Joined: 3/29/2022 Last visit: 7/25/2025 Posts: 4 Rating:
|
Olá Stefan, observei que essa CPU nova 6ES7512-1DM03-0AB0, não está listada no TIA Portal V17, onde as especificações desta, apontam somente para a V18 do Tia Portal. Porém, não sei se entendi o que encontrei, mas existe um GSD MLFB 6ES7512-1DK01-0AB0, que me parece ser possível baixar e usar essa nova CPU no tia Portal V17. Sabe me dizer se há algum Tutorial para baixar esse GSD para que eu possa trabalhar na Versão 17 do TIA Portal, com essa CPU ? agradecer se puder me ajudar. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/26/2023 08:06:40New subject after splitting |
|
| 9/25/2023 6:46 PM | |
|
Joined: 1/21/2013 Last visit: 1/13/2026 Posts: 4394 Rating:
|
P_habermann, Please post in English as this is an English language forum.
A GSD file only allows you to integrate the CPU into a file bus system, not to configure and program the PLC. This can only be done with the right version of TIA Portal, which for the 6ES7512-1DM03-0AB0 is TIA Portal V18 or newer (at the time of writing, V18 is the current version). However, since 6ES7512-1DM03-0AB0 is the successor of 6ES7512-1DK01-0AB0, you can configure the old device type and download that configuration to the new device type. However, as mentioned above, you will not be able to use the new features of the new device. This information is also included in the delivery release. Kind regards |
This contribution was helpful to
|
|
| 10/2/2023 1:16 PM | |
|
Joined: 3/29/2022 Last visit: 7/25/2025 Posts: 4 Rating:
|
Obrigado por esclarecer. |
Follow us on