(0)| 10/13/2023 8:22 AM | |
|
Joined: 6/17/2018 Last visit: 1/2/2026 Posts: 7 Rating:
|
Hello, I have experienced the same problem as I could not see the PLC type in the request for MPI addresses. It only showed add. 1 that I knew it was from the HMI, add. 2 which is the PLC but without id. type and add.3 that is IE CP 343-1 with internal MPI add. 3. The IE CP has an ethernet link via data is transfere to a higher hierarchy. So I only unplugged the ethernet cable from the IE CP and that slowed down the activity via MPI add.3. At this point I was able to see the PLC type in download area and managed to "upload the station to PG" . Kind regards to everibody ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/13/2023 09:27:40New subject after splitting |
|
Follow us on