(0)| 10/14/2023 12:37 PM | |
|
Joined: 11/13/2014 Last visit: 6/9/2025 Posts: 1 Rating:
|
Hello all, I have similar problem: I transfer some project from S7-300 to S7-1500 so I have to stay there an old HW - Moeller Rapid link motor controlers. The I changed the odl DP/ASi maters and now there are CM AS-i Master ST V1.1 3RK7137-6SA00-0BC1. In STEP the old slave is configured as AS-i A/B Slave Universal with (IO.ID.ID2, ID1, Params): 7.A.D-0-7 There are more this slaves and all is running correctly. When I add this to TIA V15.1 there is problem: Can you help me fix it? Thank you. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/16/2023 08:57:05New subject after splitting |
|
Follow us on