(0)| 10/15/2023 4:21 PM | |
|
Joined: 6/7/2012 Last visit: 6/12/2025 Posts: 12 Rating:
|
Hi there, TIA Unified Panel (MTP1200) V18.0.0.1, opening screen as popup with a faceplate in it. The faceplate "Interface" includes 2 Text_List Resource items. The text indexes are only refreshed, if the faceplate is displayed. If text index is changed and the popup with the faceplate is opened subsequently, the texts in the I/O fields remain unchanged. I have to close the popup and reopen, then the texts get updated.
Is there a known solution, or should I quickly rework the complete philosophy of the application ? Thank you! EDIT: Faceplate is placed in a ScreenWindow of one of the Screens, not in popup. The texts in the faceplate show every time the indexes "one step" older !!! ------------------------------------------------------------------------------------------ |
Last edited by: trapper66 at: 10/16/2023 04:30:16Last edited by: Jen_Moderator at: 10/16/2023 10:04:16New subject after splitting |
|
Follow us on