(0)| 11/2/2022 1:51 AM | |
|
Posts: 1 Rating:
|
Hello, I have two problems using TSEND_C, TRCV_C in communication. Please follow attached files. one thing, when I use that function the array of data is change, (switched?) something that I set parameter wrong? How I do exchange receiving data with sending data identically?(Split? and exchange? need some advice) The other thing, I removed all the function, and all the block. and then remake the function becase of the problem I mentioned. Then TRCV_C occurs error 16#803C. I changed both ID form 1 to 4, It still happens. still not receiving data. Please help. Thank you all in advance. regards, AttachmentScreenshots.zip (584 Downloads) |
Last edited by: Jen_Moderator at: 11/02/2022 13:19:48All files attached as zip file. |
|
Follow us on