(0)| 6/9/2009 3:33 PM | |
|
Posts: 2 Rating:
|
Hi Eastern thanks for your answer; However I have read from PCS7 Engineering Manual (http://support.automation.siemens.com/WW/view/en/36050990 section 4.8.7) and it says that it is not possible to change configuration parameters in RUN with ET200S (only add a completely station); I tried to do it with the PLCSIM (no with real modules because we haven't bought them yet) and it seems to work (no error message appears). I would like to know if somebody have tried to do this on real hardware (configuration change of a ET200S input or output channel using CiR); Please imagine the following situation: You have to connect a new sensor to a free AI HF Channel (6ES7 134-4MB02-0AB0) that was previously configured as a 4-20 mA (4 Wires) input, but you found out that the new transmitter is a 4-20 mA (2 Wires) and want to do this change without stopping the CPU (we will work with a AS S7-416-2 and PCS7 Cemat). All your comments are welcome. |
Follow us on