(0)| 11/3/2023 10:35 AM | |
|
Joined: 11/12/2014 Last visit: 12/10/2025 Posts: 12 Rating:
|
I have the same problem but error give status 8005 0000 when I try to connect to server of S7 1212. The same client PLC has no problem connecting to S71215. Everything is in the same net PLC CLIENT S7 1512SP-1 V15.1 firmware v2.6 PLC SERVER S7 1212C DC/DC/DC (6ES7 212-1AE40-0XB0) v4.4 TIA V16 !!!no comm opc-ua!!! S7 1215C DC/DC/DC (6ES7 215-1AG40-0XB0) v4.5.2 TIA V17 Comm OK B&R embedded OPC-UA of a panel !!!no comm opc-ua!!! If anyone has some explanantion or tip to use.. Thanks Federico ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/03/2023 12:08:06New subject after splitting |
|
Follow us on