(0)| 11/15/2023 3:41 PM | |
|
Joined: 11/29/2019 Last visit: 7/11/2024 Posts: 5 Rating:
|
Hello all, I am having a strange problem with an FB on my program. I will try to make it simple When i try to monitor the code in the FB the values of some static variables are different than the values in the IDB. This happens also with temp variables. These tags are not written in other parts of the program.The FB is called only once in the program. The only workaround i could find was to select "set in IDB" or "non retentive" a very large struct data that i have in the static area. It seems that having too many tags set as "retentive" in the FB static interface generates this issue. I attach some pictures with a few lines of code as an example of the problem i am facing. I am currently using Tia V18 upd3, the cpu model is CPU 1516F-3 PN/DP,6ES7 516-3FP03-0AB0, firmware 3.0. Best regards AttachmentBug monitoring.zip (360 Downloads) |
Follow us on