(0)| 11/23/2023 9:32 AM | |
|
Joined: 9/30/2013 Last visit: 10/30/2024 Posts: 11 Rating:
|
Hello, welfi! How about your problem? Do you solve it? I have the similar one. My case: I have old PC (WIndows XP, WinCC 6.0) and new one with migrated project from old PC (Windows 10, WinCC 7.4) both with 5611 cards, sequently connected by mpi connection to the S7-300. New PC is the last in mpi line with terminator is ON on its 5611's connector. Several times a day on both PC connection with S7-300 is lost for about 5 secs, on old one all IO fileds are just grayed (according usual state display behaviour in WinCC) but on new PC also popping up dialog box with error "A SYNI error occurred in \Device\s7opciax#1: Bus short circuit or wrong transmission rate or partner device not powered up" that need to be clicked for remove it from screen. Could this to be solved? ------------------------------------------------------------------------------------------ |
Last edited by: nortsov at: 11/23/2023 10:09:07Last edited by: The Helping Hand at: 11/23/2023 10:28:46New subject after splitting |
|
| 11/23/2023 9:51 AM | |
|
Joined: 4/28/2015 Last visit: 11/27/2025 Posts: 10970 Rating:
|
Hello, if you can see, this User isn't part of Community now, sry. |
|
With best regards... |
|
| 11/23/2023 10:10 AM | |
|
Joined: 9/30/2013 Last visit: 10/30/2024 Posts: 11 Rating:
|
May be someone else could help me? |
Follow us on